Life is On Logo

Find an EcoXpert Back

 Our EcoXperts are certified in the following areas;

EcoXpert Certifications

  • Light and Room Control: These partners have proven skills and ability to deliver light and room control systems and solutions
  • BMS: These partners are specialists in the design, installation and commissioning of efficient building automation and environmental control systems.
  • Connected Power: These partners have proven capabilities to deliver simple and connected electrical distribution monitoring systems
  • Critical Power:  These partners have demonstrated the ability to deliver integrated energy and power management systems in critical applications.
  • Datacom: These partners have demonstrated capabilities to deliver network connectivity structured cabling systems.

Using the locator 

When scrolling through the map or zoom in or out, the list of locations will be updated according to the area.

 
  • Please enter your town/suburb & state, or your postcode in the search box and press Find an EcoXpert
  • To locate an EcoXpert by Certification, just press Locate an EcoXpert by area of expertise
  • To reset the map click the button See all EcoXperts
  • Click to show details for contact information on the location found and show the location on the map
  • Use the "Zoom" + and - to zoom in or out the map. Double clicking on the map will also allow you to bring
  • If you want to move around the map, press the mouse button and drag the map selection.